ECAT.ENRXWARN
Description
ECAT.ENRXWARN allows enabling/disabling warning W7011, which is triggered when Rx data is received from the EtherCAT master before the drive finished preparing its TX data within a sync0 cycle.
-
- This warning will not be triggered when running at 250 μs cycle times as it is normal for the TX data to be from the prior cycle at this rate..
Value | Description |
---|---|
0 | W7011 cannot be triggered |
1 | W7011 can be triggered |
Versions
Action | Version | Notes |
---|---|---|
Implemented | 02-06-03-000 | - |
General Information
Type |
NV Parameter |
Units |
N/A |
Range |
0 to 1 |
Default Value |
1 |
Data Type |
Integer |
Variants Supported
Fieldbus variants: AKD2G-SPE
Fieldbus Information
Command |
Index |
SubIndex |
Data Type |
Units |
Float Scale |
Access |
PDO Mappable |
---|---|---|---|---|---|---|---|
ECAT.ENRXWARN |
4300h |
07h |
Unsigned8 |
- |
- |
Read/Write |
No |